AnsweredAssumed Answered

Serial bus S1 makes scrolling glitchy on MSO-X-3000

Question asked by tk123 on Feb 26, 2015
Latest reply on Apr 1, 2015 by davidbottorff
Hi,

I did a single capture 20ms long (2ms/) on all channels (4+16) with an SPI serial decode. When I come to review the waveforms, scrolling is very glitchy/jumpy for time bases of 200us/ or slower. For 100us/ or faster the response is fine. Also turning off serial decode makes this annoyance go away.

It's not a new bug as I've noticed it a long time ago. I'm running the latest 2.38 firmware.  

Outcomes