I want to test run an ADS deck provided as an example to show a ADS EM solved layout can be used as a component in circuit simulation. I got the error below.
It seems the pin number of the EM component is the total port number(=10). However in the EM layout view, the actual pin number is bigger 36(greater than port number).
How to fix this?
Thanks,
(stdcmds.ael line 229, column 30)
Failed to create netlist:
In design `MyLibrary_lib:AC_PDN_Impedance_v1:schematic':
The instance `I__8' has 10 pins, but the view `MyLibrary_lib:PDN_with_Trace_v1:emModel' requires 36 to 37 pins.