AnsweredAssumed Answered

Quasi-Peak Detector Card (HP 5062-1983).

Question asked by tonyk100 on Dec 5, 2014
Latest reply on Dec 9, 2014 by tonyk100
I have just acquired a Quasi-Peak Detector Card (HP 5062-1983). 

Is it the same as 11946-60002 ? 

Does anyone know if this card can be fitted to a HP 8591A as "Option 103" or does it only fit other models in the 8590 series? 

If so, does it just slot into the card cage or are there additional connections and modifications required (I expect I will need to fit a speaker)? 

I already have the QP driver card and the driver instructions, and have searched the internet but there does not appear to be any instructions available for how to install the card. 


Thanks in advance 

Tony  

Outcomes