AnsweredAssumed Answered

How to use the N5242 IVI driver function in MATLAB instrument control box

Question asked by michael2018 on Aug 25, 2014
Latest reply on Sep 10, 2014 by ChengNing
I connected Agilent N5242A network analyzer to my computer through USB cable.  I am able to communicate to N5242A from computer through MATLAB instrument control tool box by using  Agilent IVI driver ( AqNA ). Inside the IVI driver, there are many functions which can be used to control the N5242A, but I don't know the parameters which have to input the function call.
for example: 
function [pReceiverPortVal, pSourcePortVal] = channelmeasurementgetsparameter(obj, RepCapIdentifier)
what is the obj, and RepCapldentifier.

function channelsegmentaddcenterspan(obj, RepCapIdentifier, CenterVal, SpanVal, NumberOfPointVal, IFBandwidthVal, PowerVal, TimeVal)

what are " obj, RepCapIdentifier, CenterVal, SpanVal, NumberOfPointVal, IFBandwidthVal, PowerVal, TimeVal " what value they should be? 

There are many function included in the  AqNA, IVI drivers. 
where I can find the information about which parameter should go into this  each function, which kind data will come out this function call and what functionality of each function?  What document?  

Outcomes