AnsweredAssumed Answered

Spectrum Analyzers - Why use Min Hold trace detector

Question asked by SteveReeves on Aug 7, 2014
Latest reply on Nov 9, 2015 by rftester
I notice that many of the Agilent (HP, Keysight) spectrum analyzer models have a Max Hold and Min Hold trace detector.

What examples of measurements are useful using the "*Min Hold*" function?

Also, when measuring phase noise - which type of detection should be use: Max Hold, Min Hold or Trace Averaging?


Steve

Edited by: Steve Reeves on Aug 7, 2014 9:25 AM  

Outcomes