AnsweredAssumed Answered

Benchlink III Questions

Question asked by bravenrace on Aug 5, 2014
I just switched from II to III and have a couple questions:

1.  Is there a function for adding user defined events while scanning?  I used to use this feature frequently, and now cannot find a way to do it.  For clarity, what I want to do is add notes at certain intervals based on observations while scanning. 

2.  Is there a way to name or rename chart pages?  I'd like to add a descriptive name instead of just chart 1, 2, 3, 4.

3.  Is there a way to rename a configuration?

Thanks in advance for the help!  

Outcomes