AnsweredAssumed Answered

differential signals saving with oscilloscopes

Question asked by Owen002 on Sep 17, 2014
Latest reply on Sep 17, 2014 by algoss
Hi,

I want to use two channels to measure a differential waveform and save it to the harddisk with a DSO 9254A. In "Analyze -> Math" the option "Subtract" has to be chosen and Function 1 is used. The problem is, there is only the option "On-Screen Data" available while saving. Why is it so? Is it possible to save all the data at all?

Owen  

Outcomes