AnsweredAssumed Answered

Using the MSK_Mod and FM_Mod model in ADS for envelope simulations

Question asked by Ibkay on Jan 14, 2015
Latest reply on Jan 16, 2015 by Ibkay
Hello everyone,

I'm trying to use the bundled MSK_Mod and FM_Mod models (under the Timed Modem palette) in ADS for some envelope simulations. As a starting point, I just set up a very simple circuit to verify that the output generated by the models are as expected. However, it seems I'm unable to get any output at all. I've attached the test setup schematics.

For the FM_Mod model, it is a very simple model with a single input and a single output, but I'm still unable to get any output, there seems to be something missing or fundamentally wrong with my test setup but I've not been able to figure it out.

A similar case occurs with the MSK_Mod model (please refer to the attached test schematics).

Any ideas, suggestions or corrections are appreciated, thanks!  

Attachments

Outcomes