I have couple old "artifact" :) 54832B oscilloscope that have firmware A.02.30. I wonder what latest firmware I can load on that units?
Both of them running " latest" Windows98 and both of them have Pentium II with 256MHz RAM ( not sure what the clock of the CPUs)
I also wonder if I can add more RAM to this units, and what type of memory should I used.
I am looking in to manual and one of the pic showing the motherboard. This thing look like standard ATX motherboard from end of 90s. It is passible to swap that to something newer, of the shell, that have sufficient number of standard PCI buses?
Regards.
Correction: the Windows 98 reporting that it is Pentium II, however when I run CPUID utility it saying that it is 1GHz Pentium III.
Edited by: mirek on Nov 14, 2014 10:55 AM
Both of them running " latest" Windows98 and both of them have Pentium II with 256MHz RAM ( not sure what the clock of the CPUs)
I also wonder if I can add more RAM to this units, and what type of memory should I used.
I am looking in to manual and one of the pic showing the motherboard. This thing look like standard ATX motherboard from end of 90s. It is passible to swap that to something newer, of the shell, that have sufficient number of standard PCI buses?
Regards.
Correction: the Windows 98 reporting that it is Pentium II, however when I run CPUID utility it saying that it is 1GHz Pentium III.
Edited by: mirek on Nov 14, 2014 10:55 AM
1. 2.41 was the final rev for win98.
2. from 2.30, u need to upgrade to 2.40, first...
3. this stuff is no longer posted anywhere that I know of...
new mobo?
that won't work.
upgrade to winXP?
you need more RAM that that mobo would accept,
AND...
a SCOPE SPECIFIC ISO image, which again, is no longer available.
just installing a regular copy of XP WILL NOT work.
but... these scopes still have trade in value! (if they are functional)
http://www.keysight.com/find/trade
I suggest: Www.Keysight.com/find/S-series