AnsweredAssumed Answered

IChannels3 missing from 835x.tlb

Question asked by andeezlemoyo on Nov 13, 2014
Hi All,

I am working with an 2-port E8362C, running firmware version, A.09.42.22. 

I noticed that the IChannels3 interface is missing from the 835x.tlb file.  This is a fresh and clean installation of the PNA proxy. The 835x.tlb file is installed on the remote PC when I run the proxy installer.

Shouldn't the IChannels3 interface be in there?  I don't know what else is missing, if anything. 

However in my interop dll , the IChannels3 interface does appear. 

I noticed 835x.tlb was missing the IChannels3 interface when I look at it using Visual Studio 2012 custom component set view in the VS object browser.

Thanks for the help,

Andy  

Outcomes