Dear All,
We are using Agilent DSOX2000A Series Oscilloscope in our test system for performing BER test (Bit Error Test) through Mask testing option in the scope. At present we have routed the signal to oscilloscope Channel-1 and perform the BER test programmatically using LabVIEW test code. Now we are in need to do BER measurement for two signals. My question is, Is it possible to route my 2nd signal to Channel-2 and perform BER test for both the signals (in Channel-1 and Channel-2) simultaneously using the test code. Attached a screenshot of our existing LabVIEW VI (for Channel-1 mask test). Please share your inputs. Thanks in advance.
Note: Both the signals are in same Freq and Amp (square pulse) so could use the same mask file for both the signals
Best Regards,
Sathish kumar D
We are using Agilent DSOX2000A Series Oscilloscope in our test system for performing BER test (Bit Error Test) through Mask testing option in the scope. At present we have routed the signal to oscilloscope Channel-1 and perform the BER test programmatically using LabVIEW test code. Now we are in need to do BER measurement for two signals. My question is, Is it possible to route my 2nd signal to Channel-2 and perform BER test for both the signals (in Channel-1 and Channel-2) simultaneously using the test code. Attached a screenshot of our existing LabVIEW VI (for Channel-1 mask test). Please share your inputs. Thanks in advance.
Note: Both the signals are in same Freq and Amp (square pulse) so could use the same mask file for both the signals
Best Regards,
Sathish kumar D
I don't know about Labview, but the scope can do it by using "Test All" in the Mask Setup Options menu. When on, it will compare all waveforms on the screen with the mask.
You can overlay Ch1 and Ch2 inside the same mask if they are identical and need to undergo the same test, or you can build two separate mask cutouts for the two signals using custom regions.