AnsweredAssumed Answered

voltage measurement in DC electronic load HP6060B

Question asked by oren on Feb 5, 2015
Latest reply on Aug 6, 2015 by MattC
I am using the HP6060B to characterize the discharge curve of a Li-ion battery.  I see a correct current measurement of 0.5A when setting that as the desired load current in the constant-current mode, but I do not get the correct voltage reading on the LCD or through the GPIB interface.  It is showing only 0.01V instead of 3.7V.   What am I doing wrong or misunderstanding?  

Outcomes