AnsweredAssumed Answered

simple question about the design parameter.

Question asked by wangyiliu99 on Oct 27, 2014
Hi, 

I have a simple question about the design parameter in ADS schematic. 
Assume I have a three-layer schematic, 
I have one parameter P1 defined as P1=1 on the top level;
then after pushing into 2nd hierarachy, I define P1=2; 
Then click into 3rd hierachy, define P1=3.

If I run the simulation at the top level, where P1=1. Is it true that the simulation is done with P1=1? Or it is done with P1=2 or 3?

Thanks for the help!

BR,
Yiliu  

Outcomes