AnsweredAssumed Answered

Measuring hollow rivet inductance with HP 8753B @2.4GHz

Question asked by ON1EV on Dec 10, 2014
Latest reply on Dec 23, 2014 by ON1EV
Hi ,the community , I would like to measure the small hollow rivet inductance  used to make via's in an small power amplifier @2.4GHz(1w) the dimension is the following diameter 1.5 mm lenght 2 mm, I have a HP 8753B to make the measurement , after measuring the value found are more important than the value given from the formula from PUCEL and Goldfarb 3.0, the formula gives  a value of 267 pH and the VNA 500 pH, please find enclose  the document  that described the mode of measurement.
Every information will be grateful 

Guy 
ON1EV  

Outcomes