AnsweredAssumed Answered

DSA90804A local programming

Question asked by grzegorzgrzeda on Sep 11, 2014
Latest reply on Sep 15, 2014 by algoss
Hello, 
I've been recently writing a program for a host computer, which comunicates with the oscilloscope through LAN and aquires the MEAN and STD of some measurements (which involved communicating with a generator with USB/UART converter). I've been wondering is there a way to write a simple program in C/C++ (with simple shell interaction) and copy it to the device to run it locally. I saw the GUI generator, but my question is: is there a SDK or something I can use to comunicate directly with the "oscilloscope program" on the device? It could speed up things a bit and most of all I wouldn't have to use another computer. 

Regards
Grzegorz Grzeda, PL  

Outcomes