AnsweredAssumed Answered

Cant Identify instrument on remote GPIB connection.

Question asked by redhed on Sep 4, 2014
Latest reply on Sep 11, 2014 by redhed
I am Using ACE on windows 7 in an attempt to talk with an E5071C analyser and eventually integrate it into a c program i am writing.
I have managed to acquire a PNA-L remote GPIB connection in my software and ACE.
When i attempt to connect to the ENA type analyser it can connect to the remote interface i have setup over the LAN with the correct IP address however no instrument can be identified. 
I have selected the same address as what is written in the analyser for the talker/listener connection, still no response from the device.

Any help would be greatly appreciated. 

Thank You  

Outcomes