Dear Sir,
I have converted the project from ADS2009 to equivalent workspace in ADS2011.10. I used the ATF54143 transistor in ADS2009 and easily generated the layout for ATF54143 transistor.
In ADS2011.10, how to generate the layout for ATF54143 transistor.I tried, right click on the ATF54143 transistor and selected the component and latter chosen the component. Later I am not able to find the SOT343 in the component art work .
In ADS2011.10 , how to get the SOT343 in the component artwork.
Attachment is shown the selection of component artwork of ATF54143.
I have converted the project from ADS2009 to equivalent workspace in ADS2011.10. I used the ATF54143 transistor in ADS2009 and easily generated the layout for ATF54143 transistor.
In ADS2011.10, how to generate the layout for ATF54143 transistor.I tried, right click on the ATF54143 transistor and selected the component and latter chosen the component. Later I am not able to find the SOT343 in the component art work .
In ADS2011.10 , how to get the SOT343 in the component artwork.
Attachment is shown the selection of component artwork of ATF54143.
Attachments
When we right clicked on the schematic of ATF54143 and selected the component > Edit Component Artwork , Later we went to the compent artwork. In the component artwork, it is only showing the Default.It is not all showing Fixed and also it is not allowed to browse for selecting SOT343. What I have to do, how to get in the component network type to fixed.
If we generate the layout for the ATF54143, it is showing strange shape in the layout.
Attachments
As you said, I did it.I have got the layout generation for ATF54143 with two MLIN's,but layout is not generated in a proper manner. Schematic of ATF54143 with two MLIN is different, layout generation is different.It is generated the improper layout for ATF54143 with two MLIN's
Now I am getting twice generation of same ATF54143 transistor layout in the layout view, how to get the single layout generation of ATF54143 transistor layout in the layout view.Twice generation of ATF54143 transistor layout is showed in the screen shot.
How to generate the proper layout generation with all pins of ATF54143 with two MLIN's.
Screen shots are shown with schematic of ATF54143 with two MLIN's,and improper layout generation.
Edited by: nimbargi on Aug 14, 2014 12:52 PM
Attachments
http://www.edaboard.com/thread321281.html