AnsweredAssumed Answered

WaveGen Disabled On Menu Entry

Question asked by sineforbrains on Feb 25, 2015
Latest reply on Feb 26, 2015 by infinite.persistence
I have an MSOX-4034A. Things are good with the WaveGen except for the fact I cannot initially enter the wavegen menu with the output disabled. This is a problem if I have a load attached but wish to change the settings before turning on the output. Of course I can disconnect the load, enter the WaveGen menu to adjust it, and then reconnect the load, but that is annoying and can cause unneeded wear to the BNC connector.

Is there anyway to enter the WaveGen menu initially without turning on the output?  

Outcomes