AnsweredAssumed Answered

Query: Calibration-Response thru SCPI command

Question asked by geetak on Jan 2, 2015
Latest reply on Jun 2, 2015 by geetak
Hi,

I am using Network analyzer: E5071C
I have query on SCPI command(using LabVIEW) to zeroing the power level while trying to use the cal method as response(Thru)

Manually same thing will be set as below:

Cal>>Calibrate>>Response(Thru)>>SelectPorts(2,1)>>Thru>>Done

I tried to find the equivalent command using the help available in keysight website:
http://ena.support.keysight.com/e5071c/manuals/webhelp/eng/


Soft Keys on Network anaylzer:     Equicvalent SCPI
Select Ports      :SENS1:CORR:COLL:THRU 2,1
Thru                     :SENS1:CORR:COLL:THRU 2,1;*OPC?
Done                     :SENS1:CORR:COLL:SAVE"


I will configure the required config as below 

:CALC1:PAR1:DEF S21
:SENS1:SWE:TYPE POW
:SOUR1:POW:STAR -45
:SOUR1:POW:STOP 5
:SENS1:FREQ 2620000000
:SENS1:SWE:POIN 201
:SENS1:BAND 1E3

Then try to run the command 
:SENS1:CORR:COLL:THRU 2,1
Getting an error : *Additional standard needed.*

Please help me to find the right way to execute the Cal>>Resp(thru) method using LabVIEW or SCPI command set.

Thank You in advance!.

Regards
Geeta Kannammanavar  

Outcomes