AnsweredAssumed Answered

AgNA IVI usage with M937XA

Question asked by alan001 on Oct 28, 2014
Latest reply on Oct 31, 2014 by alan001
Just getting started with the M937XA and have been reading the online help manual at "http://na.support.keysight.com/pxi/help/latest/help.htm".  At the same time I am attempting to code up some basic measurements using LabWindows/CVI 2013 and the AgNA IVI driver interface.  For the most part I can relate the instrument operations to IVI function calls and Attribute settings.

At this point, the one thing I cannot seem to find in the IVI library is is the method to set "Search Domain" or "User Span" limits for marker searches and trace statistics.  For example, I am trying to use the trace statistics to get p-p ripple over a specified span without limiting the trace sweep to the same span.

Any help or examples would be appreciated  

Outcomes