AnsweredAssumed Answered

Converting cal files for different VNA

Question asked by chrisran on Jan 8, 2015
Latest reply on Jan 8, 2015 by bhokkan
I'm using an 85056A 2.4mm cal kit with an 8722ES VNA, but the cal kit was originally for an 8510 and I'm unable to read the coefficients from the disk into the VNA.  The 8722 sees the file on the disk but cannot read it.  Is there a way of accessing the cal files (converter for instance) so that I can manually load them?  Thanks.  

Outcomes