AnsweredAssumed Answered

T406 Defective VTEP probe, use "verify all mux cards" to debug 1 6.

Question asked by darek on Dec 20, 2014
Latest reply on Jan 5, 2015 by dbailey
Hello,

Many of times I have an issue for 2 of our fixtures.
Directly after vectorless test is starting I'm getting an error:

"T406 Defective VTEP probe, use "verify all mux cards" to debug 1 6. "
or
"T406 Defective VTEP probe, use "verify all mux cards" to debug 1 3." 

That issue coming during first test cycle directly after fixture lock. 

1 solution) After few times fixture lock/fixture unlock, fixture start working correctly.
2 solution) If I run software directly in BT-Basic window and then I back to operator window Medalist, then vectorless test start working without cycle fixture lock/unlock.

Because both solution above work for me then I can exclude hardware issue. 

Do you have any idea what could be a reason?

Regards
Darek

Edited by: Darek on Dec 20, 2014 5:03 PM

Edited by: Darek on Dec 20, 2014 5:05 PM

Edited by: Darek on Dec 20, 2014 5:07 PM  

Outcomes