I'm missing the 871x Format IMPEDANCE MAGNITUDE for Z and Phase angle on my new instruments. I also don't have a old 871X book around but, in the old, antique days, you could Hit MATH Display User Defined F4 and you got Z and phase on one display, the equivalent of a vector impedance meter. I don't have that and the Smith Chart presentation is there but not exactly what I want. These 5062 units have the 250 option and, being an antique, I need some (as Spiro said) pointy headed intellectual to write the code for me. (I once programmed a simple program to do a Fibonnacci series and did 87000 lines of asterisks before the operator got back from his coffee break. I could do a root canal, myself, easier that write what I need.)
Somewhere in the big, cold world of E5062 users, someone else musta used and missed this format and I sure could use such a display.
From Bacau Romania, the flower of Romanian Moldovia--where the sun flowers really are in bloom--comes this request for help. Maybe I can get back to Dallas sooner if I can see what I want.
Thanks.
J Fred, JD, MBA
Somewhere in the big, cold world of E5062 users, someone else musta used and missed this format and I sure could use such a display.
From Bacau Romania, the flower of Romanian Moldovia--where the sun flowers really are in bloom--comes this request for help. Maybe I can get back to Dallas sooner if I can see what I want.
Thanks.
J Fred, JD, MBA
More Info on Parameter Conversions (check out page 163 of ENA-L Manual):
http://cp.literature.agilent.com/litweb ... -90060.pdf
ENA-L as VVM App Note:
http://cp.literature.agilent.com/litweb ... 3987EN.pdf