AnsweredAssumed Answered

metamaterial resonator structure stimulation using ADS

Question asked by nsm on Dec 13, 2014
Hi,

I just started working on metamaterial structures for designing patch antennas using metamaterial structures. I need to simulate the the behavior of certain resonator structures.Please see the attached file for an example. I was curious to know if we can simulate these structures using ADS or EMPRO. There is a provision to encase the substrate within a waveguide in ADS under the EM header. Can we use this. 

It would be great if somebody can suggest a method to start the simulation using EMPRO or ADS.

Rgds  

Attachments

Outcomes