AnsweredAssumed Answered

PNA-X/029 noise receiver integration time

Question asked by VANDERWAL on Nov 10, 2014
Latest reply on Nov 12, 2014 by Dr_joel
I was wondering, what integration time does the noise receiver of the 029 option in the PNA-X use for noise measurements?
Based on the typical noise figure trace noise of 0.07 dB, one might assume that 1 ms per frequency point is used. Is this value fixed for all bandwidths?

Furthermore, I found this in the help file:
"Increase the number of averages to reduce jitter. This also increases measurement speed."
(http://na.support.keysight.com/pna/help/latest/Applications/Noise_Figure.htm)
If only this could be true.  

Outcomes