Hello all,
I have one 53132A marked in the rear with option 012. However when I ask through SPCI *OPT? it answers me option 010. I check inside and the oscillator corresponds with the one for option 012 (Agilent P/N 10811-60260-R ). The firmware revision is 4806.
Any idea why is answering wrong ?
regards,
Jorge
I have one 53132A marked in the rear with option 012. However when I ask through SPCI *OPT? it answers me option 010. I check inside and the oscillator corresponds with the one for option 012 (Agilent P/N 10811-60260-R ). The firmware revision is 4806.
Any idea why is answering wrong ?
regards,
Jorge
I am not sure why it is implemented this way as it is confusing. The *OPT? command returns the following (pg. 4-134 in the Programming Guide) based on the options installed: