AnsweredAssumed Answered

PNAX win7 vs winxp UI differences

Question asked by rok on Mar 3, 2015
Hi,

I'm transitioning over to the new Windows 7 version of the PNA-X with firmware A.10.25.02. In the Windows XP version, for a state file with multiple windows, there use to be a small gray rectangular box in the top left hand corner of each window that would clear itself when the measurement for that window was done. But in the Win 7 version, it seems to have disappeared. Can that feature be reincorporated into the win 7 version, or is there another visual way to determine which window is the current running measurement and what windows have completed the measurement?

Thanks,
rok  

Outcomes