Question 1:
In my PXB with options 612, 634, JFP and QPF with N5106A-031 (QTY=2) and using the Fade (ext in) configuration and FW 2.2.1.3. How do I sum the outputs of the two faded channels?
I see in the simulator there is a partial way using configuration "1 Channel + Summed Interferer" or Single-User MIMO (ext in) 2x2, 2x4, etc but these require very expensive upgrades? I want to create and inject the interference source externally using a N5102A interface from my FPGA card and not use the PXB internal AWG or -EFP upgrade option. The attached picture shows what I would like.
Is there another configuration that will allow fading and digitally summing using external inputs?
Question 2:
The website shows option N5106A-FFP as "Discontinued". Is Keysight not supporting signal capture in the PXB product anymore?
In my PXB with options 612, 634, JFP and QPF with N5106A-031 (QTY=2) and using the Fade (ext in) configuration and FW 2.2.1.3. How do I sum the outputs of the two faded channels?
I see in the simulator there is a partial way using configuration "1 Channel + Summed Interferer" or Single-User MIMO (ext in) 2x2, 2x4, etc but these require very expensive upgrades? I want to create and inject the interference source externally using a N5102A interface from my FPGA card and not use the PXB internal AWG or -EFP upgrade option. The attached picture shows what I would like.
Is there another configuration that will allow fading and digitally summing using external inputs?
Question 2:
The website shows option N5106A-FFP as "Discontinued". Is Keysight not supporting signal capture in the PXB product anymore?
Attachments