AnsweredAssumed Answered

BenchVue, Resolution

Question asked by franklin on Aug 25, 2014
Latest reply on Sep 8, 2014 by robint
When measuring a 10 V DC transfer reference with the 34461A, there seems to be a higher resolution in BenchVue compared to the DMM. The DMM’s resolution is 10 µV while BenchVue displays a resolution of 1 µV. When exporting data to Excel, there is even a 0.1 µV resolution. Is this real and if so, is it reliable? It would be interesting to get some views on this and possibly an explanation.  

Outcomes