AnsweredAssumed Answered

PNA-X Receivers IP2,IP3 and TOI performance

Question asked by andyTPE on Dec 6, 2010
Latest reply on Dec 6, 2010 by daras
Can anyone provide me with some typical numbers for the PNA-X receiver linearity.  I understand that these parameters are currently not spec'd, but I would really appreciate even some ball-park numbers for:
Receiver IP2 under single tone input
Receiver IP3 under single tone input
Receiver TOI under two tone input (I think the PNA-X app note mentions ~+26 dBm)

..or a pointer to where I could find such info (other than measuring them on the unit I have....)

Many thanks

Andy  

Outcomes