Hello Mr and Mrs
i would like to ask how to activate the speaker icon on the spectrum analyzer N9340B. Each time i used the Spectrum Analyzer N9340B for the fieldstrength measurement, the audio can't come out from the speaker even i tried to connect it with headset. is there any software that i should install first? . if there are, may i know the price?
thank you for the answer
Best Regards
i would like to ask how to activate the speaker icon on the spectrum analyzer N9340B. Each time i used the Spectrum Analyzer N9340B for the fieldstrength measurement, the audio can't come out from the speaker even i tried to connect it with headset. is there any software that i should install first? . if there are, may i know the price?
thank you for the answer
Best Regards
This is from the Chinese support node:
"The speaker on N9340B can output the demoded AM or FM signal, and the operation process is as below:
1) connect an antenna which can cover about 100 MHz signal. (to demod FM signal).
2) set the center freq to a FM signal freq (for example 101.7 MHz at my site).
3) Press [SPAN]->{Demod}->{FM on}->{Delay time 10 second}->{Speaker Vol 80}; You can hear the voice of FM output from the speaker, and of course you can plug the headset too."
I hope this helps.