AnsweredAssumed Answered

Use E5052B to retrieve screenshot from E4440A via intuilink

Question asked by d_finz on Jul 24, 2013
I have a multi-instrument test setup that includes among other devices an E5052B and E4440A.  I don't have a compatible printer that will work with the E4440A (can't find printers anymore that have parallel ports!) so I'm now considering using intuilink to download screenshots from the E4440A.  However, before I run out and purchase a computer I wanted to see if I could install intuilink onto the E5052B.  I figure that since the E5052B runs on Windows and has a GPIB port then intuilink should work fine.  Any input/advice would be greatly appreciated!

-Dan  

Outcomes