Are there any difficulties to replacing a FPGA chip heatsink from the 16754A LA board?
I have (re)applied several times the thermal paste and the heatsinks for normal GPUs and CPUs
but I was wondering if the outer/edge paste for these FPGA heatsinks is some special glue paste.
I have (re)applied several times the thermal paste and the heatsinks for normal GPUs and CPUs
but I was wondering if the outer/edge paste for these FPGA heatsinks is some special glue paste.
That card was discontinued sometime in 2005, and went 'Out of Support' in August 2010. Agilent's manufacturing has moved in the meantime, so chasing down old manufacturing processes may not be possible.
Al