AnsweredAssumed Answered

read marker values on Smith chart of E5061A

Question asked by iee488 on Jun 17, 2014
Latest reply on Jul 19, 2017 by spidermonkey1187
Have only 1 channel and only 1 trace.

The marker displayed has value:  0.000 s  -995.67 mOhm 194.70 Ohm 2.4059 uH

I can read the 0.0000 s with the :CALC1:MARK1:X?  query
and I can read the next two resistance values with the :CALC1:MARK1:Y? query

But I cannot figure out which query to use to read the inductance.

Help appreciated.  

Outcomes