... is this possible somehow?
I use currently one N5182A to generate a reference clock (491.52MHz) for an RF setup and another one to supply test input. This will be LTE but for testing I put in just some CW (e.g. 2330 MHz). However, I need them to be stable.
I use currently one N5182A to generate a reference clock (491.52MHz) for an RF setup and another one to supply test input. This will be LTE but for testing I put in just some CW (e.g. 2330 MHz). However, I need them to be stable.
The easiest way to get them stable is to connect the 10 MHz Out from one signal generator to the 10 MHz In of the other signal generator.
Another method is with option 012.
The following application note discusses the two methods. http://cp.literature.agilent.com/litweb/pdf/5990-5442EN.pdf
Regards -