AnsweredAssumed Answered

Integrating N67xx modules into N6700 mainframe

Question asked by Cynthia Employee on Jan 7, 2014
Latest reply on Jan 10, 2014 by MattC
Hi,

I came across a clause in the N6700B manual which states that
"Modules must be installed next to one another, starting with slot 1. Do not leave any empty slots between modules..." 

Can you explain why we are not allowed to just put 1 module on slot 2 or slot 3? What about those modules that take up 2 slots and why are these modules able to work?

I thought I have tried with modules at just any slots before and it works. Is this all the while like this or it was a newer of firmware that does not allow this to happen? Or perhaps I was just imagining.

Thanks.

regards,
Cynthia  

Outcomes