AnsweredAssumed Answered

8712ES Question

Question asked by 8510fan on Jul 23, 2010
I recently purchased a 8712ES on EBAY in Inop condition, the unit had a issue with the CPU board but i was able to get a new CPU board from another guy on Ebay, unfortunatly i made a "dog induced" mistake when entering the Serial# so now i got a messed up SN in the board !
The service manual mention that there is a reset code which clears the SN and allows reentry of the number via GPIB , does anyone know this reset code ?  

Outcomes