AnsweredAssumed Answered

34461a -- odd screen flaw after using temperature probe

Question asked by economist on Jun 23, 2014
Latest reply on Aug 10, 2014 by guidow
This is odd. I was just attempting to measure temperature using the probe from my Fluke 289. Apparently it's not accepted by the 34461a. But that's not my problem. Right after attempting the measurement (and getting "-OVERLOAD" as a result), I now have a horizontal white line on my display that won't go away. It's approximately in the middle of the screen and remains after reboot, full power down, etc. I can even see it on the very first boot-up screens. Any ideas? I can't imagine using the wrong temp probe would cause a hardware flaw, but I guess it's possible. Anyone have any ideas?

Edited by: economist on Jun 24, 2014 12:26 AM  

Outcomes