AnsweredAssumed Answered

add a pin though ael script

Question asked by wizardyhnr on Jan 21, 2014
Latest reply on Jan 22, 2014 by wizardyhnr
i am trying to add a pin though ael script in ADS. one problem is about the angle calculation. 

if you add a pin through the built-in icon, ADS will calculate the angle automatically and make sure 90 degree angle between the pin and edge which the pin is attached. 

so i am wondering if there is some ael algorithm that can implement the angle calculation.

anyone can help me?

thanks!  

Attachments

Outcomes