AnsweredAssumed Answered

Problem with tracking generator HP 70300A

Question asked by Hifreak on Jul 8, 2013
Latest reply on Jul 19, 2013 by dhamilton
Hello All,

I have a complete HP 70000 series spectrum analyzer to 22 GHz with the HP 70300A tracking generator to 2.9 GHz.

I have tested the tracking generator and above the 2.4 GHz is the tracking generator output unleveled.

The error code is: ERR 2008 70300A 6.19.

Has somebody an idea of the error or an adjustment manual to recalibrate the tracking generator?

I am curious about your reactions.

Regards,
Marcel  

Outcomes