Here's more info about this obsolete model, 8648B special handling option H31.
Option H31 is to move the Pulse Input Connector from the rear panel to the front panel and guaranteed max. power output => 16dBm when combining with option 1EA and 1E6.
It's located at the top right on the front panel. Please refer attached photo.
Here's more info about this obsolete model, 8648B special handling option H31.
Option H31 is to move the Pulse Input Connector from the rear panel to the
front panel and guaranteed max. power output => 16dBm when combining with
option 1EA and 1E6.
It's located at the top right on the front panel. Please refer attached photo.