AnsweredAssumed Answered

Noise Floor Simulation Help

Question asked by vivian on Jun 27, 2014
Latest reply on Jun 30, 2014 by aehoward
Hi,

Question regards to noise floor calculation in ADS.
The components in the behaviour model that have a noise parameter associated with it has be set to YES and temperature set to 16.85C (290K). Also, an Options have been added to set the simulation and model temperature. However, the noise floor ADS calculated does not match the Receiver Noise Calculation = kTBF, ADS shows -90dBm...? 

Thank you,  

Outcomes