I'm trying to create a AM output signal with the N5181B MXG analog signal generator but when I try to configure a there is a message "feature not available" or "option not instal", I search in the Agilent web and I not could find information about this. In the manual tells "option UNT installed", this is about some kind of program or driver?
I will thank any kind of information.
I will thank any kind of information.
The N5181B will not have AM, or any analog modulation unless Option UNT is installed.
The way to verify that you have, or do not have Option UNT is to do these keystrokes:
Utility -> Instrument Info -> Options Info -> Instrument Options -> Turn the Big Knob on Front Panel to highlight Option UNT.
Option UNT will be installed only if the word Permanent appears under the Expiration column and a check mark is next to its description. See screen shot example attached.
Regards -