AnsweredAssumed Answered

Play two following sequences without using a third sequence (N5182A)

Question asked by antoine on Jun 27, 2013
Latest reply on Jun 28, 2013 by tabbott
Hello everybody,

I have some sequences which have a number of segments (ARB waveforms) close to 1024, thus I can not do a new sequence of these to play them one after another.

So I would like to play these sequences one after each other, I am using the SCPI commands to control the generator and I already try to do it with a "List Sweep" but it seems it works as a new sequence so the number of segments is to high to do it work like that.

Do you know if it is possible for example to send a command which says: "Play this 1st sequence" and then to send a new command while playing the sequence 1 to say: "When you finished to play your actual sequence, play this new one (sequence 2)"?

Thanks for your help,

Antoine  

Outcomes