AnsweredAssumed Answered

Spurious waveforms while loading

Question asked by 3lionsct on Jan 8, 2014
Hi,

Is there a way to shut off the output of a 33500 while loading waveforms using Waveform Builder Pro?

I've noticed that when I download a waveform, the unit outputs the "EXP_RISE.ARB" file which is one of the built-in functions at a level that appears to be related to the amplitude of the last waveform sent to the unit. This could have a really bad effect on the amplifier I am driving

I hope there is a work around because I do not want to have to write my own program to download these waveforms which shuts off the output while loading

Thanks  

Outcomes