AnsweredAssumed Answered

DSAX96204Q RiseFall Time Threshold Percent Remote Setting Command

Question asked by shaobing on Jul 2, 2014
Latest reply on Nov 7, 2014 by rab82001
Hi,

I use the command ":MEASure:THResholds:RFALl:PERCent CHANnel1,80,50,20" to remote control the rise/fall time threshold percent from default 90%/10% to 80%/20%. However, the scope does not respond. Could anyone figure out the problem or provide a correct command?

Thanks  

Outcomes