AnsweredAssumed Answered

comparsion between SMC+phase and VMC measurements

Question asked by nsm on Sep 12, 2013
Latest reply on Sep 17, 2013 by Dr_joel
hi,

I am trying to measure the conversion phase of mixers and these are double balanced mixers from 2 to 18GHz. I also need to compare the phase response of the mixers with respect to one another to group mixers that have the least deviation amongst them.

Can this be done with the SMC+phase measurement methodology?

If I were to measure SC21(Phase) using the SMC+phase and measure the VC21(Phase) using the VMC method, will the phase response be the same?


Rgds  

Outcomes