Hello,
Can anybody guideline me, or have experience in building a high power test set using the N5230C PNA-L.
Way to setup a system and calibration.
Regards,
J
Can anybody guideline me, or have experience in building a high power test set using the N5230C PNA-L.
Way to setup a system and calibration.
Regards,
J
Extra information about what I like to do.
I like to add an external test using some external couplers that can handle higher powers then the internal coupler in the PNA-L N5230C (with option 146 and 080)
+ a booster amplifier using to drive my DUT (= amplifier).
One way to do this is by connecting the coupled port of each external coupler to the measurement receiver of the PNA-L
(with some attenuation between the coupled port and the receiver to protect the measurement receiver, and not to go in compression)
But if I do this, I assume, that a need to write my own calibration routines. Correct?
Anybody experience?
Regards,
J.