i want to set the hotkey of ADS layout,
but, only can use one letter?
for example,i user the letter "D" to set the menu "edit"->"delete" hotkey, yes,i works!
but,if i want to use two letters as the hotkey, how can i do it?
but, only can use one letter?
for example,i user the letter "D" to set the menu "edit"->"delete" hotkey, yes,i works!
but,if i want to use two letters as the hotkey, how can i do it?
Accellerator keys can be multiple characters, for example Alt-E and then D will invoke the Delete command, but these are defined in the sequence of the equivalent menu label strings and are not configurable by the user.
In ADS 2011.01 and later there is the addition option of the Layout Command Line Editor. This has many editing functions defined with two letter mnemonics, e.g. Delete is defined as de. Most common functions are already defined but the user can also define additional functions as required.