AnsweredAssumed Answered

Calibration using E-CAL with extra cables an adapters.

Question asked by rohit on Feb 24, 2014
Latest reply on Feb 25, 2014 by rohit
Hello Friends,

Attaches is the word file which will explain the my measurement setup and its related query.

The basic problem which i am facing is, I will have to do the characterization of extra cables and adapter which will not be there in actual measurement setup but in order to do calibration and connect E-Cal I need to use the extra cable and adapters. Is there any standard procedure/steps to do this.
                            I have heard about characterizing the extra adapter which we need to do if we don't have same ports on DUT and E-CAL,could something similar be used here with the extra cables too.

Any help will be highly appreciated. :) 

Thanks & Regards,
Rohit.  

Outcomes